Hello,
I'm planning to use the OPA830 to drive a clock signal over 50 Ohm coax. The datasheet shows data on VS = +/-5V, 5V and 3V but not for 10V. It does however state that it supports up to a single ended value of 11V.
1. Can a 6 to 11V supply be used and will it allow me to have an output range of 0 to Vs? (not exactly Vs but I assume within a few hundred millivolts)
2. I need to generate a level from 0 to 6V. Is this possible on the output?
3. Is the maximum input 3.2V? I have an option for the input to be 3.3V, I'd like to keep the gain down in order to have greater bandwidth.
Note, the web bench tool indicates that the max single supply is 5.5V which conflicts with the datasheet.
thanks,
Adam