Other Parts Discussed in Thread: TINA-TI,
Is there a plot available for current noise density vs frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greg,
Since the input current noise spectral density is a function of the input bias current (Inoise=sq-rt(2*q*IB), in the case of CMOS and JFET (OPA827) input op amps it is very small and thus in most cases may be neglected. However, you may still simulate it using our Tina-TI macro-model available on our website - see below. The increase in the Inoise above f=100kHz as shown in the graph below is caused by the interaction of the input capacitance and open-loop output impedance. I have attached the simulation file for your own simulation.
In CMOS and JFET input amplifiers like OPA827 there is 1/f component in the input voltage noise spectral density but no 1/f in the input current noise spectral density.