This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM6171: LM6171 output waveform issue

Part Number: LM6171


Hi team,

The customer is using LM6171BI for the integral circuit application. He uses two LM6171 devices. The input signal is the sine with amp=1Vpp,

f=5KHZ. The power supply is +/12V. He measures the output signals through the oscilloscope. Please check the fig 1. The green waveform is

the input signal. The yellow waveform is the output waveform for U1 which is in my TINA circuit. The blue waveform is the output waveform

for U2 which is in my TINA circuit. From the output waveform, the yellow waveform is the sine  and it is fine. But the blue waveform is

not the sine waveform. It is not integrating at all. 

Then follow the customer's circuit, I design a TINA circuit. From the output waveform, the output waveform for U1 is fine, it is also the sine.

But the output waveform for U2 is bad, it is not the sine. Please check the fig 2. Then I change the R4 value. When I select 1K,10K or 15K

for R4,  the output waveform for U2 can be fine. The fig 3 is the output waveform when R4 is 15K. But when R4 is more than 20K, 

the output waveform for U2 will be bad.  

Q1: So, I would like to know why I reduce the R4 value, the output waveform for U2 can be fine. My Tina circuit is also in the attach.

Q2: If I change R4 to bellow 15K value, the U2 output waveform will be fine, is this solved the customer's issue?

                                                                                                      fig 1

 

                                                                                                     fig 2

 


                                                                                                    fig 3

LM6171.TSC

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments