Hello team,
I am looking for an Op Amp where the VCM can go somewhere in between 200 and 300 mV below the Negative Voltage Supply, and it should apply over a temperature range -40°C to 85°C
Other relevant specs: BW can be as low as 1 MHz, Supply Voltage is 3.3 V, Offset Voltage < 1 mV, RRIO.
I found OPA342 at 300 mV (as well as a few others at 200 mV), but they only spec the VCM for TA = 25°C