Other Parts Discussed in Thread: TINA-TI, , ADS1274
Tool/software: TINA-TI or Spice Models
Hi,
In my application I need to measured 24 bit analog input, low frequency signals. For that purpose, I thought to use the ADS1274 Simultaneous Sampling, 24-Bit Analog-to-Digital Converters with the THS4521 sigma delta ADC Drivers (according to the Figure 89 in the ADS1274 datasheet).
- Problem 1: In my application I'm using the THS4521 with gain 1 configuration which has 145MHz gain at 0dB. When I'm trying to calculate the total noise (broadband, flicker…), I'm getting very high noise values as "Noise Bandwidth" (BW sub n) so the total noise is very high (assume brick wall factor 1.57). I notice that in Figure 89 you used a 1.5nF capacitor for, I'm guessing, low pass filter, right? What is the cutoff frequency?
- When using the TINA TI simulation for noise analysis (attached herewith, figure 89), I need to connect the "rg1" left signal to something. I tried to connect it to Vcom (2.5V) but I getting errors in DC analysis first. How can I connect this leg in order to perform the Noise analysis?
Thanks,
Idan sbom341d.tsc