Other Parts Discussed in Thread: TINA-TI, , LMP8672, LPV802, LPV542, LMH6724, TLV8544
Tool/software: TINA-TI or Spice Models
Hello Precision Amplifiers Forum,
This may belong in the Simulations and Models Forum, but I believe this forum will best answer my immediate question/concern.
I have been very hard pressed to find a model of the TLV8542, simply because I need it in some sort of library/component form so that I can use it in a circuit board design. The only models offered on the TI site are a .LIB file, which is the library extension for KiCad. When attempting to import this LIB file into KiCad there is an error that is just a Chinese character. The only other option is the SPICE model which I wouldn't mind having because I like the ability to model things in SPICE before building them.
My second issue is with this SPICE model. Model is a strong word, it is technically only a schematic (.TSC), but when this schematic is opened there is a basic circuit with a component labeled as TLV8542. I assume this is where the data from the TLV8542 datasheet was generated, since there is also a graph representing Gain vs Frequency. The problem is that in this SPICE schematic this component is NOT TLV8542, under the properties it is LMP8672.
The question: is LMP8672 even close to a valid representation for TLV8542? I would argue that the simple fact that LMP8672 is not RRIO and TLV8542 is RRIO would massively impact all of the simulated models.
I need to use TLV8542 very specifically in an RRIO setting, and I would like to model it in SPICE using the most basic Bubba Oscillator circuit. Are there any suggestions on components that actually exist in SPICE that would be viable representations of the TLV8542?
Best regards,
Michael Slitts