Hello,
I use OPA355 in an high impedance non-inverting input stage: at the inverting input, I have the feedback resistor Rf=200ohm, and a resistor to GND Rin=1k.
At the non-inverting input, I have a resistive divider of 637k to Vin and 363k to GND. the OPA355 is supplied +3V and -2.5V.
The stage is supposed to withstand an input voltage (Vin) range of +/-60V, even if saturated for high voltages. When V+ tries to pass 3.5V or -3.1V, I expect the ESD diodes to open and clamp the voltage. The ESD diode current should stay below 60V/600k=0.1mA.
This works as expected for negative voltages, but it does not work for positive voltages. The circuit behaves as the diode from the non-inverting input to the positive rail would be missing.
Furthermore, I repeated the experiment with the unpowered OPA355. The rail voltages stay relatively low (few hundreds milivolts), due to other loads on these rails.For negative input voltage, the non-inverting input voltage clamps at 0.5V below the negative rail, as expected.
However, for positive input voltage (up to 60V), the non-inverting input voltage does not clamp and goes up to +8V. This permanently damages the OPA355, by increasing the offset voltage. The offset voltage grows with the stress amplitude and duration.
Is this expected behavior?
Is this something I do not understand in the data sheet?
Thank you,
Best regards,
Mircea