I am seeing what appear to be stability issues with OPA2227 amplifiers.
The circuit is a simple inverting circuit (non-inverting input ground), gain -1, with +/-15V supplies. Input and feedback resistor 10K, and 33pf between output and inverting input.
There is 100mVp-p at 100MHz on the output, which is only visible with an active probe. If you add a little capacitance to the output (e.g. a passive probe the noise goes). Just to confirm this is causing offset errors in circuits connected downstream, which go if you connect a passive probe to the inverting circuit output.
Also, not all OPA2227 amplifiers show this problem, usually replacing the device fixes it.
Has anyone else had this problem?