The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA270A-Q1: the Max Full Range Offset +- 3mV is applied at the fixed Gain = 14 ?

Part Number: INA270A-Q1
Other Parts Discussed in Thread: INA270, INA271

Hi Team

may I get your quick response ?

INA270A-Q1 has Max Full Range Offset = +- 3mV and Gain = 14[V/V].

customer wants to know the max offset at the fixed Gain = 14[V/V].

the Max +- 3mV offset is applied at Gain = 14[V/V] ?

or I has to calculate Max +- 42mV offset by (3mV x 14) ?  

I believe INA270(Gain 14) and INA271(Gain 20) have the fixed gain respectively,

so that the Max full range offset is applied at the fixed gain,

but I need BU's confirm.

  • Hey Paul,

    You are right. The +-3mV is the specification for the amplifier’s input offset (Vos). This is why we label the specification “Vos, RTI”. RTI stands for “referred to input”. RTI Vos error is modeled as positive voltage source on non-inverting terminal. Thus, in order to determine the Output offset, you multiply RTI Vos by the gain.

    Analyzing error (including Vos) is discussed in our training video series here: training.ti.com/getting-started-current-sense-amplifiers

    Sincerely,
    Peter Iliya
    Current Sensing Applications