Other Parts Discussed in Thread: LMH6723
Hello,
I'm currently using the LMH6654 in a prototype Load Transient Circuit for testing high power regulators. The amplifier drives a discrete AB output stage which then switches some load FETs on or off. The current setting pulse is provided by a function generator and a 25mV input corresponds to a 25A load step at the output of the regulator under test. GaN transistors were chosen for the load FETs to keep input capacitance down and provide faster switching.
Currently, I can get a positive slew rate of ~140A/µs for a 50A step (50mV input pulse) but I'd like to push that higher if possible. Is the LMH6654 the best choice for this application? I picked it for the high GBW and decent output current drive but if there's a better amp our there I'd be happy to use it instead.
Thanks for the help!
Carmen
Schematics attached.