Hi all
Would you mind if we ask TLV4172?
<Question1>
There is the description "The input range can be extended beyond (V+) – 2 V up to V+. See the Typical Characteristics and Application and Implementation sections for additional information."
What does it mean "The input range can be extended beyond (V+) – 2 V up to V+."?
Common-mode voltage range should be range (V-) - 0.1 to (V+) - 2V.
Is it possible to use (V-) - 0.1 to (V+) with normal operation?
<Question2>
There is the description on the datasheet P1 as follows;
"The input can operate 100 mV below the negative rail and within 2 V of the positive rail for normal operation.
Note that these devices can operate with a full rail-to-rail input 100 mV beyond the positive rail, but with reduced performance within 2 V of the positive rail."
In case of beyond common mode voltage range, we assume that the output will be saturated with V+ or V-.
It is not normal operation. So, that's why, it is not "with reduced performance", right?
Kind regards,
Hirotaka Matsumoto