Other Parts Discussed in Thread: ISO1541, TIDA-00313, INA226, TIDA-01608, ISOW7842, INA260, OPA333, TIDA-00528, TIDA-00332, INA138, AMC1100, AMC1200, INA149-EP
Hi All,
URGENT!!
I want High side current monitor, low voltage current sense amplifier having following specifications
Load current to be monitor > 15A
Input voltage = 400V
Common mode voltage 400V, which is equal to bus voltage.
I have find the different technique to increase the common mode voltage range but it add lots of error in output. So please suggest any better solution for the same.
Thanks
Prashant