Other Parts Discussed in Thread: TL072
To TI Support Team:
For the base part TL071xxx series (regardless of package type), we need to know if the Input Clamp Current specification of -50mA can be exceeded for a short time? The customer is using an input that may briefly spike a bit past that on the input from time-to-time on start-up for a few milliseconds or so, does not want to activate the input's ESD clamp, and so was wondering what the peak surge spec was for short time periods?
Can you help us with this? Can you provide the peak surge value for short time periods for Input Clamp Current spec on base part TL071xxx and email the answer to me at dan.rapp@mouser.com?
Thanks!
Dan Rapp
Technical Support
Mouser Electronics
(800) 346-6873
(817) 804-3800
www.mouser.com
Q9B8030