Part Number: INA2332
Hi everyone,
I am having some problem with output with the INA2332 based bridge amplifier.
Differential inputs(pin2 of all Header3) are connected together with one bridge circuit using Variable Resisters.
Common mode voltage is 2.5V and differential voltage is 2mV.
I expect the outputs(VoutA and VoutB) show same voltage or slicely different, but they show large difference voltage as one is 2.62V and the other is 0.49V.
If I increase the input differential voltage, the two output voltages increase linearly.
Of course, the values of resisters are checked.
What could be the reason for this difference?
Thanks in advance.