I have connected as per datasheet,but voltage was not varying for varying frequency.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
the above pictures are for 100 rpm with input wave form and output voltage of the Lm2907N
the above pictures are for 1000 rpm with input wave form and output voltage of the Lm2907N .
the above pictures are for 3000 rpm with input wave form and output voltage of the Lm2907N .
for all the rpm frequency input was varying and output voltage was same as attached .please suggest .I am using 8 pin only .
Hi Kai,
Thank you for your suggestion.
Still i didn't get complete solution. As per your information i have done ,it worked really well.In out put the voltage level getting saturated after 1.7Khz (Say 10.7V after which it remains same for all frequency). Still i am working on it.