Part Number: BQ500100
Other Parts Discussed in Thread: BQ501210
Hello
we have a setup with a WPC transceiver with enabled FOD, pretty similar to the BQ501210 dev kit. Now we have a WPC receiver from Rohm. Without the FOD enabled we can transfer up to 10 W without any problem. But with the enabled FOD we are not able to transfer more than 5-6W after this we receive a FOD warning. We have the feeling that the Current measurement has too much noise / ripple on the I_SENSE line. What are good values for the RF and CF? In the datasheet there is 1 Ohm / 0.1 uF, in the dev kit it is 10 Ohm / 1 uF, what are the differences between these two possibilities? What are the advantages / disadvantages?
In the datasheet it is stated that when the output ripple is > 30ms the RO / CO values shall be changed. In which range is it meaningful to modify this? What are the advantages / disadvantage when we change the RO value from 1 kOhm to for example 10 kOhm?
Thank you ver much for your support
Best Regards
Lorenz