This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA827: The output voltage question for OPA827

Part Number: OPA827

Hi team,

I have a question for 5.1. TI Precision Labs - Op Amps: Bandwidth 1.  In this video, the input signal frequency is 200kHZ, the closed gain

is set to 100V/V. The GBW for OPA827 is 22MHZ. So, 200kHZ*100V/V=20MHZ<22MHZ, So, the 200KHZ input signal can be 

normally amplified 100 times. That is  when the input signal is 200KHZ, the closed gain should be 100V/V, correct?

But in TINA circuit, it shows the closed is 37.75dB when the input signal is 200KHZ. Would you explain this?