Part Number: LM324A
Other Parts Discussed in Thread: LM324, LM2902K, LM324K, LM358
Hi Support team
May I know the Vf of Internal clamping diode
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Red,
Only LM324K and LM2902K have an ESD cell on the input pins. All LM324 variants have a parasitic diode as part of the PNP base node.
LM324 Vf (at 25C) will be similar to this LM358 input curve. (I don't have a LM324 curve on file). The exact value is not important; the key points are that lower than -0.3V may cause output phase reversal and limit current to -1mA or less using external resistors to reduce device stress.