Other Parts Discussed in Thread: TLV6001
Hi,
The OPA348 part has internal CM and DM filters builtin , but my deisgn has external CCM ,CDM capacitors with series resistors as shown in the image.
The circuit is built for current measurement across the shunt resistor. I am using the maximum inverting Input voltage to the circuit is 150mV with the single supply of 5V. the Non inverting input is 0.
Is it really needed to have external EMI filter for the OPA348 part with the above said conditions
Regards
Gayathri