This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA548: What is the real "junction to case" Thermal Resistance Rjc value ?

Part Number: OPA548


Hallo,

2 different values are given in the data sheet. Page 5 show Rjc bottom with 0,2 K/W and Page 7 show Rjc with 2,5 K/W. What is the correct value for the heat sink calculation? TO-220-7 Package. My feeling tells me 0.2 is not enough. What is mean with Rjc bottom in detail?

Thank you.

  • Hello,

    It looks like you have identified a problem with the OPA548, 7.4 Thermal Table in the datasheet. The table lists the RθJC(bot) Junction-to-case (bottom) thermal resistance 0.2 °C/W, where it should be 2 °C/W (f > 50 Hz) as listed in the Electrical Characteristics table on page 7.

    The RθJC listed in the Electrical Characteristics table is for practical purposes the same as RθJC(bot). Newer thermal tables break the RθJC into two components; from the junction-to-top RθJC(top), and from the junction-to-bottom RθJC(bot) of the package. But for a power op amp such as the OPA548 nearly all of the heat is conducted from the junction to the bottom via that lower thermal resistance path. This assumes that an efficient heat sinking system is employed. A small amount of the junction heat is conducted to the top of the package and then radiated.

    I'll make note of the problem with Table 7.4 and we'll need to get it corrected. Thanks for bringing it to our attention.

    Regards, Thomas

    Precision Amplifiers Applications Engineering

  • Hi,

    Has this inquiry regarding the OPA548 thermal properties been answered to you satisfaction? If so, please close out this E2E inquiry.

    Regards, Thomas
    Precision Amplifiers Applications Engineering