Hello,
I was hoping to learn more about the input impedance looking into the ONET8551T from the PD (so IN/FILTER). We are intending to first design a circuit to emulate the PD current for initial tests prior to connecting the ONET8551T to the PD, and would like to ensure impedance matching. My understanding is typically TIAs are expecting the current source of the PD to look as a high impedance source. I also see from the datasheet that the recommended operating conditions are 200 fF for the PD and 0.3 nH for the wirebonds. We could use those values to get an estimate of ideal input impedance looking the photodiode, but we would appreciate any additional information that could be provided related to this, such as input impedance into the TIA and range of acceptable impedances looking from the TIA back to the PD.
Thank you,
Nathan Abrams