Other Parts Discussed in Thread: OPA2333-Q1, OPA2137,
Hi team,
Our customer is looking for low offset and EMC torelance dual opamp, because they are in trouble with the EMC test of the system.
Although they can evaluate only OPA2333-Q1 due to package circumstances, OPA2137-Q1 also meets offset requirements.
If OPA2137-Q1 has EMC tolerance equal to or higher than OPA2333-Q1, we believe that OPA2137-Q1 will become the favorite.
Is there any test result measured under the same conditions?
Or can you prove that EMC tolerance does not get worse?
Especially immunity test is assumed.
Because they can not directly evaluate OPA2137-Q1, I would like to obtain the result compared with OPA2333-Q1.
Best regards,
Tomoaki Yoshida