Hi support team experts,
My customer is having some urgent question regarding the equations in the INA282 datasheet, could you please help us to clarify them:
System Setting:
- REF1 => 0V (Grounded)
- REF => 2.495V (from TL432B)
- V+ => +5V
- Rshunt = 15mohm
- Maximum current = 15A
- Bus voltage = +48V
Question1: What is the value 12V in the VOS_CM equation ? Is it a constant value?
Question2: What is the definition of VCM in the VOS_CM equation ? Does it refer to VIN for my case?
Question3: If considering there is a ripple voltage with 4Vp-p and the dV/dt is 40V/us on VIN, how to calculate the VOS_CM which is cause by the ripple voltage?
Question4: What is the definition of VREF of VOS_REF ? For my case, REF1=0V, REF2=2.495V, how can I obtain the VREF to calculate the VOS_REF ?
Question5: What is the tolerance of 2.048V in VOS_REF ?
Thanks a lot.
Best Regards,
Wei-Hao