hi,
we are using an OPA2544 dual amplifier as Bridge Driver Circuit is shown in figure 4 in datasheet document. The power supply is ±35 V and power consumption is less than ratting. we use a good heat sink and ESD safety is taken into account, too. In this condition, one on the internal op-amps is damaged sometimes. why is that?
due to value of the absolute maximum voltage (±35), is the applied voltage (±35) high? what supply voltage should we use?
thank you