Customer is having troubles simulating the INA216A3 with INA216A3 PSpice Model (Rev. B) using PSpice A/D OrCAD Capture 16.6
They've tried to run the example sim but are getting this issue:
**** RESUMING SIM1.cir ****
.END
.SUBCKT GND_FLOAT VDD VSS GNDF
EGNDF GNDF 0 VALUE = {(V(VDD)+V(VSS))*0.5}
.END
$
ERROR(ORPSIM-16363): Command invalid in subcircuit
----$
ERROR(ORPSIM-16499): Missing .ENDS in .SUBCKT
WARNING(ORPSIM-15256): <X_U1.XU1.XU9.VMINIO> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.XU1.XU9.VMAXIO> not a subcircuit param
They also get the same error when using that specific part in the design. They've been able to add other parts of the circuit from manufacturer websites without issue.
Do you have any ideas?
Regards,
Mark