Other Parts Discussed in Thread: INA181, INA4181, INA2181, INA199-Q1, LMP8640-Q1, INA203-Q1, INA250-Q1, INA193A-Q1, INA200-Q1, INA225-Q1, INA282, LMP8481-Q1, INA270A-Q1, INA210-Q1, INA282-Q1
Hi,
We are looking for dual or quad channel high-side current sensing amplifier with either analog or SPI/I2C output.
We would like to sense the currents for the following voltages:
+9V
-9V
+4.25V
-4.25V
Current Sense Range: 0 to 1.5A
Please suggest a suitable amplifier for the above mentioned requirements.
We checked on the following IC on the TI website:
1. INA4181-Q1 (4 – Channel Current Amplifier with analog outputs) - www.ti.com/.../ina4181-q1.pdf
As per the datasheet of this amplifier, this amplifier can accept voltage from -0.2V to 26V on IN+ and IN- pins in common mode.
As per our understanding, this amplifier can be used to sense current for +9V and +4.25V. Please let us know if these devices can be used to sense current for -9V and -4.25V?
If not then please suggest similar devices to INA4181-Q1 that can be used to sense the current for the below mentioned voltages:
+9V
-9V
+4.25V
-4.25V
Current Sense Range: 0 to 1.5A
Thanks & Regards,
Sunny Watts