The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2460: Differential input voltage, VID

Part Number: TLV2460

Hi,

Please let me clarify my understanding the VID of TLV2460. I understand that the VID means that the voltage at the non-inverting input with respect to the inverting input. So it means that TLV2460 allow to input VDD+0.2V between +IN and -IN, right? For example, at VDD=5V use case, we can input 5V to +IN pin without no damage when -IN=0V. Is my understanding correct?

I'm referring following document about VID understanding.

Best Regards,

Satoshi