Hello,
I would like you to confirm whether input and output spec for TLV2401.
* According to datasheet, it seems that user can input both negative and positive supply.
However, when I check waveforms in datasheet, there is no figure in case of negative voltage input.
Then questions are below.
1. Is it possible to input dual supply in TLV2401 ? ("Vcc" pin -> Postive voltage(Ex. 4V) and "GND" pin -> Negative voltage (Ex. -4V))
2. If yes, is it correct infomation about "-0.1V to Vcc + 5" spec of "VICR" ?
Best Regards,
Machida