Hello,
I would like you to confirm whether input and output spec for TLV2381.
* According to datasheet, it seems that user can input both negative and positive supply.
And also, I can find figure which both negative and positive voltage is input .
From above two information, I assume that this device is corresponded to dual supply.
However, I have following question.
1. According to above, common mode is defined as "-0.2 to Vs+0.2", is it correct information ?
2. When user require to use dual supply, can user input positive supply to "Vcc" pin and negative supply to "GND" ?
Best Regards,