HI,
I would like to use the OPA548 as power supply with regulated voltage output from 0 to 5V and current to 3A. I am using the reference schematic from SBOS070C TI document with addition pwm adjustment for the output voltage. When i set the output (for example 4V) voltage and attache the resistor 3,3ohm to simulate load of 1,21A the output voltage drop to 3,5V. My needs is to be able to emulate lipo battery and to privide correct voltage with current support up to 2,5A. Since i get output voltage drop i can't hold output stable. I have set the current limit to 4A and power supply is 12V/5A.
What could be reason the OPA 548 to not hold the voltage output when we attache the load that require less current then the max current that OPA548 can deliver?
Best Regards,
Vlatko