This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6518: Will LMH6518 accept differential input?

Part Number: LMH6518

In the datasheet, it says:

The input is differential but is driven single-ended as long as the conditions of Table 6 are met, and there is good
matching between the driven and undriven inputs from DC to the highest frequency of interest.

I'm a little confused, is it mean "although the input is differential, but it can ONLY be driven signle-ended" or "although the input is differential, but it can ALSO be driven singled-ended"? I must make sure this, because I'm considering put another full differential amp before it.

Thanks.