Hi team,
Below is the schematic of the LMV641
In the application of my customer, the output is almost 5V, but the next stage of the output may have a signal with Vmax=10V will added in output pin(RSST_OP_RT45).
The signal is as below:
The signal frequency is about 100k and will last about several ns, the Vmax is 10V.
Customer want to know will the short high voltage signal added in the output pin do the damage in the pin?
Does the pin have the ESD to protect the shot time overshoot signal?
If so, what the maximum voltage can be tolerant?
Lacey
Thanks so much!