dear:
one of our customer need used ONET2804T on 100G Rosa, have to questions :
1. for the filter capacitor:
in the datasheet, It is recommended to use two single layer ceramic (SLC) capacitors in the range of 270 pF to 680
pF for power supply decoupling.
the range is 270~680, my question is which is the best value of the capacitors ?
2. SCL and SDA pin , these two pins must to reserved of can not used, Thanks