This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC3303: Max. Output current & Total response time

Part Number: MC3303
Other Parts Discussed in Thread: TLV4170,

Dear Sir/Mam,

Good day..!!

           I'm having doubt on MC3303D, Low power operational amplifier it have max , output current at load & total response time ?

With Regards,

Nivetha A.,

  • Nivetha,

    There is only 10k ohm load specifications for output voltage which also implies a current value. The operating characteristics table on page 4 of data sheet has slew rate , rise time, fall time typical values. MC3303 is 29 years old. There are many other newer op amps with more data sheet charts. TLV4170 is just one example.