Other Parts Discussed in Thread: OPA197
Hi team,
My customer wants to verify what is the output voltage swing and input common mode range for OPA2197-Q1 across the full temperature range(-40 ~ 125deg)?
Thank you.
Best Regards,
Wei-Hao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer wants to verify what is the output voltage swing and input common mode range for OPA2197-Q1 across the full temperature range(-40 ~ 125deg)?
Thank you.
Best Regards,
Wei-Hao
Wei-Hao,
OPA197 input common-mode voltage range over -40 to 125 deg C temperature range is: (V-)-0.1V<Vcm<(V+) - see below.
The output voltage swing is a function of output current and it ranges from 15mV from rail for Iout=0 to 500mV for Iout=9mA (RL=2k)
However, for high linearity the output swing from the rail is defined in the AOL condition column - see above.
The maximum output swing vs output current from rail over temperature is shown in the graph below: