Part Number: MC3303
In the EC talbe, it says the 10uV/degree (typ).
1. is this for full temp range from -40degree to 85degree?
2. For example to calculate input offset voltage at the specific temp:
- If temp is 60degree, the temp coefficient will be 10uV x (60degree - 25degree) = 350uV
- if temp is 0degree, the temp coefficient will be 10uV x (0degree - 25degree) = -250uV
Are above examples right? if not, how come?
Thanks.