Dear TI Sir
What's TL331 Input offset voltage range?
Below MIN show empty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Terry,
The offset voltage is typically ±2mV at room temperature (25°C) at a 5V supply voltage.
The offset voltage is guaranteed to be less than ±5mV at room temperature (25°C) at a 5V supply voltage.
The offset voltage is guaranteed to be less than ±9mV over the full temperature range (-40°C to 85°C) at a 5V supply voltage.