Hello,
I am evaluating the SN10502 for an application where short circuit and transient threats must be considered on the output pin. Since the SN10502 has no internal protection features, I have added them in the form of a series resistor, TVS diodes, and shottky diodes clamping the output to the voltage rails. To evaluate the sufficiency of my protection scheme, I would like to know the absolute maximum voltage which can be tolerated on the output pin. I did not see this information in the datasheet. Is it known?
Thanks and Best Regards!