This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1704: TLV1704 supply

Part Number: TLV1704


Dear Kai, thank you

Please, explain:  you mean that, if to feed the TLV1704 and the pull-up from different supplies, then the values of these voltages may differ. And it can lead to failure of the  TLV1704? Even, if the difference is very small - 200-300 mV?

Thank you.

Sincerely,

Vladimir Naumenkov

www.agat.by

  • Hi Vladimir,

    during power-up or power-down the voltages can rise or fall unequally. Then through the pull-up a current can be injected into the output pin of TLV1704. This need not necessarily destroy the chip, but can result in latch-up or other unexpected behaviour.

    Kai