This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV981-N: CDM and latch up current

Part Number: LMV981-N
Other Parts Discussed in Thread: TLV9001

Our customer need LMV981MFX ESD CDM level and CDM test standard ,AND latch current paremeter 

I don't see the parameters in datasheet, where can I get the parameters or reference , thanks.

  • Hi Lanjie,

    The CDM and latch-up current parameters were not tested for this device and are not included in the datasheet. If you need a similar device with specified CDM and HBM values, try the TLV9001.

    Best,
    Paul
  • HI Lanjie,

    This device is about 20 years old and unfortunately, there is no data for CDM. If you provide some further information on your application and part requirement, I can help you find a part which does specify CDM in the datasheet and meet your requirement.

    For the latch-up Current test (I-test) is at 200mA.

    Regards,

    Sanjeev