Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi,
I am working with the spice model for LMV761. According to the datasheet, recommended operating conditions for the supply are +2.7V to +5.25V, however electrical characteristics are given for +2.7V and +5V supplies only. Is the spice model defined for supply voltages between those values? My experimentation and some related posts suggest it may not be. If that is the case, is there an updated model available that is well behaved for supply voltages that are not 2.7V or 5V?
Thanks!