This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6301: Question about the Power Dissipation of THS6301IRSAR

Part Number: THS6301

Hi team,

     As customer want to know the max power dissipation of THS6301RSAR when it works, and I see dynamic power consumption and quiescent current in the datasheet. To get the max power dissipation, whether we need to add this two? for example, when THS6301 is working at the drive mode 1, the total power dissipation would be P=220mW+15.9mA*12, is it right?

Best Regards

Zhengquan Lu