Hi,
I am using LF398N in my application. I am facing issues with the output voltage of the S/H which is not going more than 3.3v.
The input is varying from 0 to 5v.
VCC is 5v.
Logic is given to switching signal whose pulse width is 1ms and period is more than 100ms.
VCM=2.5v.
The hold capacitor also holds only maximum of 3.3v. Is it not possible to get more than 3.3v output using LF398?
Thanks
Ramesh B