This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV07: Dual loop feedback and output swing limitation - TINA-TI Simulation

Part Number: TLV07
Other Parts Discussed in Thread: TINA-TI

Hi,

I've made some experimentation with TINA-TI and TLV07 model. TLV07 was powered as single-supply 0V to +15V.

According to the TLV07's datasheet, the output voltage swing limitation of 120mV should be an issue at single supply. I have tried to simulate both, dual and single feedback voltage follower and according to the TINA-TI's simulation, this hasn't been appeared as an issue. For 10mV input voltage, output was 10,033992mV (10mV + Vos). TINA-TI simulation is attached. Maybe I am doing something wrong, but from my point of view, output should be 120mV or some other non-linear value.

 

Has someone experienced this issue in real single supply application?

TLV07_Output_Swing.TSC

 

Br

Josko