Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6505: Noise during mid-range gain adjustment

Part Number: LMH6505
Other Parts Discussed in Thread: BUF634A

We're trying to add a LMH6505 to our photodiode detector to remotely control the gain, using a DAC as the control signal.  The peak voltage coming from the photodetector op amp is 1.35V, and we'd like to achieve a gain of 5x.  However, when I test the circuit, I see very noisy output in the middle of the gain range.  The extremes are OK, but the middle shows lots of noise in the Kilohertz range.  I added a capacitor to the Vg input and that helped some, but mid-range gain is still noisy.  Tried decreasing the 10u caps to 1u, but that was no help.

Is there anything I am overlooking or misinterpreting?  This is a 2 layer board, so no ground planes to be concerned about.

  • Hi Gary,

    I cannot see your schematic. Can you re-post the schematic so I can see what you are doing?

    Thanks!
    -Karan
  • Karan, I'll try it again, as my first attempt was unsuccessful...  R7 is 2K and C8 is 10pF, in case it matters.

  • Hello Gary,

    When you say the output is noisy, what is the magnitude of the noise? Can you provide maybe some scope plots? Secondly, have you measured at the output of the AD825 to make sure you have configured that correctly so we can narrow down the issue to half of the circuit?

    I am going to look over the circuit to see if I can notice any component values you might have used that look incorrect.

    Thanks!
    -Karan
  • Karan,
    I have measured the output of the AD825 op amp, and it is very clean. This was an existing product that used manually selected resistors to vary the gain, and we're switching to the LMH6505 to allow remote, DAC-controlled gain adjustment.
    I'm out of the office due to illness today, so I can't take any scope shots, but I'll do that as soon as I get back in.
  •  Snapped a shot of the scope...Noise is about 30 KHz (excluding the high freq stuff).  The 831mV level in the photo is about mid-range for the total gain.  Any suggestions??

  • Hi Gary,

    What you are seeing doesn't look like noise but oscillation. Your circuit seems to be unstable. You mentioned your output from the AD825 is clean but can you show me a scope shot of that output? Also something you can try to increase stability is to decrease the Rg resistor value to increase the gain of the device. Let me know if this helps.

    Here are some recommendations to avoid problems and to get the best performance:
    • Do not place a capacitor across RF. However, an appropriately chosen series RC combination can be used to
    shape the frequency response.
    • Keep traces connecting RF separated and as short as possible.
    • Place a small resistor (20-50Ω) between the output and CL.
    • Cut away the ground plane, if any, under RG.
    • Keep decoupling capacitors as close as possible to the LMH6505.
    • Connect pin 2 through a minimum resistance of 25Ω.

    Thanks!
    -Karan
  • Hello Gary,

    On another note, not related to your issue. I think you can use the BUF634A instead of all those components for your output stage. The BUF634A
    can be used inside the feedback loop of op amps to increase output current and replace that output stage you have setup. It provides up to 250mA output current.

    Thanks!
    -Karan