Hi, :
I please ask a question, I hope to design a circuit to convert a voltage range in 1-10V to output a current in 1m~10mA,
Can you please suggest some on this ? Can I use opa to do it ? Is it enough ?
Thank you very much
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, :
I please ask a question, I hope to design a circuit to convert a voltage range in 1-10V to output a current in 1m~10mA,
Can you please suggest some on this ? Can I use opa to do it ? Is it enough ?
Thank you very much
Hi, Kai:
I want to use it to drive a resistor, maybe not 'it', them, 3~4 parts, or more, it depends on different applications.
The original thinking is sum up the current from every transconductances, sorry, I don't know the right name, some said 'OTA' operational transconductance amplifier.
But from the datasheet, the OTA looks like different than regular amplifiers. I looked at OPA860, but the transconductance is not very linear.
I don't need very accurate, but too distort still very bad, I can't evaluate the distorted result easily.
Thank you very much
Hi, Michael:
First, thank you for answering me. In the application note
says 'The Howland current pump is usually excellent for that. Current sources are often used for testing other devices. They can be used to force currents into sensors or other materials. They can be used in experiments, or in production test. They can bias up diodes or transistors, or set test conditions. When you need them, they are useful — even if you only need them once or twice a year. '
I think this is what I need. Originally I don't know the 'But the practical problems involved are not so simple or obvious', How severe is it. <- I don't know this...so, I don't know if the choosing strategy is proper or not.
I don't know the keywords 'howland' , 'current pump' before you told me.
I need some time to study.
Thank you for the guide.
Regards.
Hi, Kai:
It's hard to answer your question, it should be concerned. But at the first, it's floating, then it's possible to ask to meet some criteria. But which criteria, it's not clear now.
But thinking the worst case, if apply the isolating voltage in safety, 2KV or 4KV...
Or...do you think except Howland (amplifiers), OTA , it's better to use other strategies/methods ? I ever though using isolators , but it needs more auxiliary power to supply the isolators.
Regards.