Other Parts Discussed in Thread: DAC9881, OPA2277, DAC9881EVM
Hello,
I am using OPA2277-EP as kelvin connection for DAC's reference voltage such as Fig.1 .
( Fig.1: OPA2277-EP test circuit ---- referenced from SLAU279A p20 )
Firstly, OPA227-EP is operated with +/- 14.5V and "positive input A" is about 5V.
My cognition is that
1.Due to kelvin connection's purpose, VREFH-F1 should be forced to 5V
2.If this circuit work normally, the current consumption should be about 800 μA per amplifier ( fortunately when I measure the current from OP_SENS_V+ , It was about 1580 μA )
However when I power up this circuit, I found that
1. VREFH-F1 can't be forced to 5V but 5.6V and finally went up slowly to 13.56 ~ 13.58 V
2. VREFL-F1 can be about 0V ( this result is ok, seems the "positive input B" is connected to AVSS )
Whether there is something wrong about Fig.1 or my cognition ?
Thank you for any suggestion and help.
BR
Wen