Hi Team,
According to the discussion in following thread, it looks TLV1701 can drive 3.3V CMOS logic properly if pull-up is smaller than 1kohm. But datasheet spec is too flexible to judge if it is possible or not. I'm just looking for low power comparator and TLV1701 looks good without the spec.
Then I have a coupe of questions to make it clear.
Can I confirm the progress of the request above? The lol vs Vol redone curves will definitely help for my business.
>We have put in a request to have these curves redone. I do not have a timeframe for that to occur at this point.
Eventually, Does VOL swing depend on Vs voltage level? or Right date below is correct?
You showed two different results in the past thread as followings. so I'm confused.
Regards,
Takashi Onawa