Other Parts Discussed in Thread: OPA171
Hello All,
I would like to understand that how unstability or oscillations at the output of OPAMP causes heating of device?
BR,
Nachiket W.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mr. Michallick,
greetings!
Yes, i see 200KHz 200mV oscillations on the output of OPA171. It is also correct that i am driving capacitive load and due to which opamp is unstable. when i introduced 47 ohm resistor at the output of OPA171 then oscillations were vanished and temperature was down to normal room temperature.
BR,
Nachiket Wawoo.