The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3012-Q1: ESD information not in datasheet

Part Number: TLV3012-Q1
Other Parts Discussed in Thread: TLV3012

TLV3012AQDCKRQ1

TLV3702QDRG4Q1

TL331QDBVRQ1

For these three Comparators, the ESD ratings have been omitted from the most recent datasheets, even though the Qualification Summary page for each device shows the following:

Qualification summary for:

TLV3012AQDCKRQ1

Note that the non-Q1 version of the datasheet does contain this information; for example, the TLV3012 datasheet www.ti.com/lit/ds/symlink/tlv3012.pdf  shows:

ABSOLUTE MAXIMUM RATINGS(1)

Supply Voltage .................................................................................... +7V

Signal Input Terminals, Voltage(2) ........................... –0.5V to (V+) + 0.5V

Current(2) .................................................. ±10mA

Output Short-Circuit(3) .............................................................. Continuous

Operating Temperature .................................................. –55°C to +150°C

Storage Temperature ..................................................... –55°C to +150°C

Junction Temperature .................................................................... +150°C

Lead Temperature (soldering, 10s) ............................................... +300°C

ESD Rating (Human Body Model) .................................................. 2000V

 

Please provide this info in Reply, and update the datasheets to reflect this information.

Thank you,

~Leonard